Rotary Field Direction


What you will find in this section:

  1. Rotary field direction
  2. Related topics

 

The digital output complies with IEC 61131-2 Type 3. It can be configured via the web server or the Modbus communication interface. 

 

Rotary field direction

 

The recognition of the rotary field direction is used to inform the digital output about the state of the application. The rotary field direction can be configured for both directions (left, right).
 

Navigation on the web server

“Digital output, Settings, “Rotary field direction” function

 

Menu: “Digital output, Settings, “Rotary field direction”
Menu: “Digital output, Settings, “Rotary field direction”

 

Status

The “Status” area shows the current status of the alarms.

Settings

Set the alarm according to your requirements.

Identifier

The identifier can be used to assign a user-specific designation to the function.

Idle level

There are two possible statuses for the idle level.

  • NC: Normally closed
  • NO: Normally open

The default setting for the digital output is NO.

Function

Select the “Rotary field direction” function from the drop-down menu.

Rotary field direction

Select the appropriate rotary field direction.

 

 


EMpro online documentation
Published/reviewed: 2026-07-10, en revision 004, Version history