Deactivating the Digital Output


What you will find in this section:

  1. Deactivating the digital output
  2. Related topics

 

The digital output complies with IEC 61131-2 Type 3. It can be configured via the web server or the Modbus communication interface. 

 

Deactivating the digital output

 

The digital output can be deactivated, so that no function is assigned to it.

 

Navigation on the web server

“Digital output, Settings“, “Deactivated” function

 

Menu: “Digital output, Settings“, “Deactivated” function
Menu: “Digital output, Settings“, “Deactivated” function

 

Status

The “Status” area shows the current status of the digital output.

Settings

Set the digital output according to your requirements.

Identifier

The identifier can be used to assign a user-specific designation to the function.

Idle level

There are two possible statuses for the idle level.

  • NC: Normally closed
  • NO: Normally open

The default setting for the digital output is NO.

Function

Select the “Deactivated” function from the drop-down menu.

 

 


EMpro online documentation
Published/reviewed: 2026-11-10, en revision 005, Version history