Data Exchange Settings
When you start the export in the ECAD system, you can define the following settings for the export:
| Export setting | Description | ||
|---|---|---|---|
| Sources | Select the source application (EPLAN Electric P8 or EPLAN Pro Panel) from which you want to export the data. | ||
| Import data from cxE after editing | Select whether you want to re-import your changes into the ECAD system.
In cxE, an additional ribbon section is displayed from which you can either send back the data to the ECAD system or decouple the project from the ECAD project.
|
||
| clipx ENGINEER target version | Select the target application (web application or desktop application) to export the data to. The selected application is automatically launched when you start the export. | ||
| Devices to be exported | Select the elements configured in your ECAD project you want to export.
|