Getting Started with cxE
As a first-time user, you might find the following information useful:
Do I need a cxE user and how do I get one?
You need to be registered with Phoenix Contact to exploit the full range of cxE features.
Coming from PROJECT complete planning
Some information on the differences in the UI and the availability of functions....
The user interface
A general overview on the different windows and views and what you can do there....
Application Settings and defaults
You might want to change some default values before you start working. If you want to exchange data with other applications like EPLAN Electric P8, you need to install the corresponding interface first.
All set up, you can start working by creating or opening a project.