The content you are viewing is tailored for Lithuania. View Content for United States | Choose Another Country

Heavy-duty connectors for measuring and testing tasks in the field of protection technology

2024-07-30
HEAVYCON TSC contact inserts for transformer testing

The new HEAVYCON TSC contact inserts from Phoenix Contact are used in medium-voltage switchgear. They are specially designed for measuring and testing tasks and provide a robust solution for temporary or continuous connections.

The industrial connectors ensure the reliable transmission of power, data, and signals even under difficult conditions. With the new fixed-position and modular TSC contact inserts, testing can now also be performed reliably on current transformers. The leading, automatic transformer short circuit provides maximum safety. Thanks to the robust connector housing and high IP protection, the connector is also suitable for permanent use at the control cabinet. Modular versions also make it possible to combine different transmission media in one connector, thereby creating a customized, space-saving interface. Push-in Technology saves time with its easy, tool-free conductor connection. The HEAVYCON TSC contact inserts are the answer to the increasing requirements in modern protection technology and provide a future-proof solution for electrical engineering specialists.

Press Contact
Eva von der Weppen
Eva von der Weppen | Corporate Communications