The CHARX control modular AC charging controllers from Phoenix Contact are the centerpiece of an intelligent and sustainable charging infrastructure for mode 3 electric vehicle charging. Software release 1.7.0 gives the scalable portfolio an extended range of functions through WLAN capability and other features for increased installation and maintenance convenience as well as more security.
News Keep up-to-date with the latest news about our products and technologies, our company, our strategic business development, and our sustainable commitment. You can download press information and image material conveniently in the download area.
- Filters:
-
Field
-
Event category
-
Product category
- Applied Filters (1):
Function extensions for AC charging controllers: WLAN capability and other features
Vehicle charging controllers as an interface solution between the DC charging station and the electric vehicle
The independent vehicle charging controller CHARX control vehicle from Phoenix Contact enables DC charging via CCS charging inlets for electric vehicles and utility vehicles.
NACS is coming and Phoenix Contact is ready: AC charging cables for 50 A and 80 A available from the end of 2024
As a specialist in e-mobility charging technology, Phoenix Contact will be offering the first SAE-compliant and UL-certified NACS charging cables for AC currents up to 80 A at the end of the year.
Compact CCS type 1 charging cables – the ideal charging solution up to 125 kW
The DC charging cables in the CHARX connect compact family from Phoenix Contact have been extended to include the new 125 kW performance class.
Type 2 CCS charging cables in the new housing design – robust, easy to maintain, and well-thought-out
The new generation of the proven CHARX connect standard CCS charging connectors from Phoenix Contact is suitable for setting up DC charging stations and covers the medium power range from 150 to 250 kW (150 to 250 A/1,000 V). In the new housing design, the product family offers many improvements in terms of robustness, safety, billing, and maintenance.
RFID reader for AC charging controllers with LED indicator and buzzer
The new RFID reader with configurable LED indicator and buzzer from Phoenix Contact is used in conjunction with the CHARX control modular charging controllers and is suitable for mounting in home chargers and charging stations.
Universal CCS charging inlets – charging now possible with a permanent 375 kW
The CHARX connect universal CCS vehicle charging inlets from Phoenix Contact now also enable High Power Charging with a permanent 375 kW.
Uncooled GB/T DC charging cables with CE certification for permanent charging with up to 250 kW
With the new CHARX connect standard generation of GB/T DC charging cables, Phoenix Contact offers a CE-certified charging cable in accordance with the latest Chinese GB/T standard 20234 for the global e-mobility market and corresponding applications.
Phoenix Contact E-Mobility continues to expand in China
Phoenix Contact is expanding its e-mobility production capacities with a new facility in Lishui, China. Following on from the Chinese headquarters and another production site in Nanjing, this is the Phoenix Contact Group’s third plant in China.
Convenient AC distribution module for 19" charging stations
CHARX power distribute, the new distribution module from Phoenix Contact, supplies all of the components in a 19" charging station. The incoming AC mains voltage can be distributed to up to five power modules. It also supplies power to the control module. Integrated protective functions ensure the maximum safety of downstream modules and cables.
Space-saving EMpro DC energy meters for tamper-proof measurement and precise billing
The new compact EMpro DC energy meter from Phoenix Contact enables the space-saving, precise, and tamper-proof direct measurement of currents and voltages of up to 650 A/1,000 V DC.
The all-rounder in 19-inch format: CHARX control integrated DC charging controller for fast charging stations
The CHARX control integrated DC charging controller from Phoenix Contact combines all functions for controlling and monitoring a 19" charging station in one device.