Le contenu que vous consultez est sur mesure pour France. Consulter le contenu de États-Unis | Sélectionner un autre pays

Worker assistance software for terminal strip assembly in control cabinet building

2024-09-24
clipx Engineer assemble software on the monitor

The clipx Engineer engineering software from Phoenix Contact optimizes data consistency from the circuit diagram to the finished control cabinet. The new clipx Engineer assemble worker assistance software is designed for the assembly process of terminal strips.

It can be integrated into the engineering software as a paid add-on and provides all the necessary data from the engineering process for assembly. This enables seamless integration into existing workflows. With direct data transmission from engineering and the consistent provision of all necessary production data, users benefit from significant time savings. The intuitive user interface guides you through terminal strip assembly, including accessories and markings, and supports you with clear step-by-step instructions and visual aids. This increases efficiency and reduces search times and errors. The software also offers the option of directly controlling a pick-by-light system. The correct selection of the required items is displayed for each assembly step, which further reduces the error rate.

Press Contact
Eva von der Weppen
Eva von der Weppen | Corporate Communications