Le contenu que vous consultez est sur mesure pour France. Consulter le contenu de États-Unis | Sélectionner un autre pays

Monitoring surge protection for signal interfaces

2023-09-26
Remote signaling modules monitor the surge protection for signal interfaces of the CLIXTRAB product family

Signal lines are like nerve tracts in technical systems. Therefore, it is very important to protect these system parts from surge voltages caused by switching operations or lightning strikes. The surge protective devices of the TERMITRAB complete product family from Phoenix Contact enable this protection to be realized while saving space at the same time.

Often, the protective components are installed in several control cabinets or in the field. This means that it is very time-consuming or even impossible to gain a permanent visual check of the protective devices on site. The remote signaling modules of the TERMITRAB complete product family enable you to visually monitor up to 50 surge protective devices. The devices record the status of all the protective modules and, in the event of a fault, output an alarm to a central signaling contact. In addition, these remote signaling modules can also be used to monitor the surge protective devices of the CLIXTRAB family.

Press Contact
Eva von der Weppen
Eva von der Weppen | Corporate Communications