Le contenu que vous consultez est sur mesure pour France. Consulter le contenu de États-Unis | Sélectionner un autre pays

Electronics housings for sensor and IIoT applications

2024-08-27
Overview of the three sizes of the Monitoring Case System (MCS)

Phoenix Contact offers a well-designed housing for diverse electronics with its new MCS series. It is sure to impress at all stages, from installation of the PCB and simple mounting to maintenance of the device. Modular in design, the housing offers exceptional practicality.

The Monitoring Case System (MCS) is ideal for field devices used in sensor technology as well as for IoT and IIoT applications. Featuring IP65/IP67 degree of protection, the housings are suitable for industrial use. An IP40 version is available as an alternative. The angled housing edge enables almost horizontal mounting of the PCB. This feature enables the preassembled connectors to glide through the holes in the housing. This means that the maximum PCB floor surface can be the same as the housing base surface, achieving maximum use of the installation space. In practice, the electronics housing impresses with its additional hinges. These hinges are subsequently inserted into the housing and connect the upper housing part and the cover to the lower part. This leaves your hands free for maintenance or installation work. The seal is also connected to the housing in such a way that it cannot be lost.

Users combine standard components, optional accessories, and our comprehensive portfolio of connection technology to create a wide range of solutions for their application. The MCS is available in three sizes as well as with various frame and cover versions. In addition, the housings can be customized with printing and marking options as well as mechanical processing.

Press Contact
Eva von der Weppen
Eva von der Weppen | Corporate Communications