Le contenu que vous consultez est sur mesure pour France. Consulter le contenu de États-Unis | Sélectionner un autre pays

Connectors for motor connection of blinds, window coverings, and awnings

2024-02-20
Connectors for motor connection of blinds, window coverings, and awnings

Phoenix Contact’s QPD STAK 3 and QPD STAS 3 installation connectors designed for assembly simplify electrical installation. They have been specifically developed for the motor connection of blinds, window coverings, and awnings.

The power connection is implemented quickly and easily on the field side with the QPD STAK 3 connector. The QPD STAS 3 connector is used on the device side. IDC insulation displacement connection technology facilitates convenient assembly, as it eliminates the need for special tools and stripping. Electrical installation is completed safely and without errors in no time at all. The installation situations, which are often difficult to reach, require a connection that is not only simple, but also robust and durable. The QPD STAK/STAS 3 installation connectors are designed to meet these requirements. The splash-proof and dust-proof housings provide a high level of protection in outdoor applications, are resilient against tensile load, and impress with their shock resistance. Even extreme temperatures or UV rays cannot harm the power distribution.

Press Contact
Eva von der Weppen
Eva von der Weppen | Corporate Communications