Requirements on e-invoices and invoice quality
The quality of your invoice is the basis for our processing. In particular, this ensures the contractual payment of the invoice amount.
- The correct order number is listed on the invoice. If possible, the order number should be listed separately without any other information added to it.
- The invoice meets the requirements of VAT law.
- The invoice contains the gross, net, and tax amount.
- The invoice address is the same as the invoice address noted in the purchase order.
- Submit the original invoice in single copy. Do not send us copies of invoices.
- The invoice must have a legible print quality. Choose a white background if possible.
- Note your vendor number on the invoice.
- The invoice must specify the quantity, unit, unit price, and net total value.
- Specify the currency in ISO code (e.g., EUR).
Registration and submission process
Before sending e-invoices, you must follow the designated registration and reconciliation process. Please send the required information to purchase@phoenixcontact.com and then use the invoice recipient address designated for the respective Phoenix Contact company.
Please designate a departmental contact person for the e-invoicing process, as well as one or more central, non-personal sender addresses from which invoices will be sent to Phoenix Contact.
Important information regarding submission
- Only one invoice document may be submitted per e-invoice.
- The email serves solely as a means of transmission; what matters is the structured invoice data.
- Invoices must be sent to the correct invoice recipient address for the respective company.
- Invoices from portals or downloads should be avoided whenever possible and are permitted only as a special process following prior approval.
- Additional supporting documentation or documents relevant to the audit may not be accepted as an alternative special approach without prior approval.
Specifying shipping and freight order numbers
Shipping numbers, freight order numbers, and freight forwarder numbers are to be provided as additional logistical references and are not to be used as the order number.
Additional requirements for the exceptional case of an invoice without a purchase order reference
Invoices without a corresponding order reference are permitted only in justified exceptional cases. In this case, you must specify the full name of the requester.
In addition to the general quality requirements, you must also specify one of the two following Phoenix Contact-specific references in the structured data section of the e-invoice:
- Email address of the requester (e.g., john.smith@phoenixcontact.com)
- Cost center of the requester (e.g., cost center 108000)
Handling incorrect e-invoices
Any incorrect or incomplete e-invoices and any that cannot be processed for technical reasons may be rejected. This applies in particular to invalid formats, structural or syntactic errors, missing required information, incorrect document types, unclear service periods, missing order references, and discrepancies between structured data and the view document. If errors occur repeatedly, clarification with the appropriate contact person will be necessary.