Wiring Current Transformer


What you will find in this section:

  1. Pin assignment example
  2. Related topics

 

warning signDANGER: Risk of electric shock

If the device is disconnected, the secondary side of the relevant current transformers must be short circuited.
Install the current sensors and corresponding measuring devices only when the power supply of the system is disconnected.
When the current transformer is operated with an open secondary circuit, hazardous voltages may occur at the secondary terminal blocks.

 

information sign

When measuring by means of current transformers or Rogowski coils, the accuracy is greatly influenced by the quality of the current sensors used. current sensors used. 

Pin assignment example

 

information signMaximum tightening torque for the relevant screws: 0.5 Nm ... 0.6 Nm.

 

Pin assignment example (with current transformer)
Pin assignment example (with current transformer)

Hint: This image shows an example of EEM-MA370

 


 

 

See also

  1. Mounting

 


EMpro online documentation
Published/reviewed: 2025-07-15, en revision 003, Version history