Connecting Supply


What you will find in this section:

  1. Schematic for connection types
  2. Related topics

 

warning signDANGER: Risk of electric shock

If the device is disconnected, the secondary side of the relevant current transformers must be short circuited.
Install the current sensors and corresponding measuring devices only when the power supply of the system is disconnected. When the current transformer is operated with an open secondary circuit, hazardous voltages may occur at the secondary terminal blocks.

 

Schematic for connection types

Power supply option - Low-voltage grids:

You can connect the device supply as follows:

  1. Connection L/N (AC)
  2. Connection L/L (AC)
  3. Connection +/- (DC)

 

Power supply option - 24V DC:

 

 

See also

  1. Mounting

 


EMpro online documentation
Published/reviewed: 2026-11-10, en revision 005, Version history