Device Status


What you will find in this section:

  1. Device status
  2. Related topics

 

The digital output complies with IEC 61131-2 Type 3. It can be configured via the web server or the Modbus communication interface. 

 

Device status

 

The “Device status” function can be used to check whether the device is on or off.

Here, it is also possible to define whether the output is normally closed (NC) or normally open (NO) in idle state. 

 

Navigation on the web server

“Settings, Digital output”, “Device status” function

 

Menu: “Settings, Digital output”, “Device status” function
Menu: “Settings, Digital output”, “Device status” function

 

Status

The “Status” area shows the current status of the digital output.

Identifier

The identifier can be used to assign a user-specific designation to the digital output.

Idle level

There are two possible statuses for the idle level.

  • NC: Normally closed
  • NO: Normally open

The default setting for the digital output is NO.

 

 


EMpro online documentation
Published/reviewed: 2026-07-10, en revision 004, Version history