Rolling Average Value (Rolling Block)
What you will find in this section:
Rolling average value (rolling block)
|
Interval with rolling block |
There is a set interval and a subinterval. The subinterval has to be an integer factor of the interval. Example: If the selected interval is 15 minutes, three 5-minute subintervals have to be selected to match it. The average value is generated and updated at the end of each completed subinterval. |
Related topics