Average values
What you will find in this section:
Average values
The device makes it possible to determine average values based on the available measurement data.
The average is generated for the following measurement values:
- Voltages: phase to phase U12, U23, U31
- Voltages: phase to neutral conductor U1, U2, U3
- Frequency
- Currents I1, I2, I3, IN
- Active power: consumption, supply
- Reactive power: consumption, supply
- Apparent power
The measurement values are divided into groups. These groups can be configured independently of each other.
The following groups have been formed:
- Voltages
- Frequency
- Currents
- Power
- Predictions
For each average value, the minimum and maximum averages are always recorded and displayed. The data can be called up via the web server, the display and via the communication interface.
The times (Unix time stamps) of these recordings are stored device internal. These can be all called up via communication interface. For the values of power measurement these are also shown on the display directly below the respective value (as soon as a value has been calculated). The minimum and maximum average values can be reset.
Related topics