Operating Hours Counter
What you will find in this section:
Operating hours counter
|
Navigation on the display |
“Device info, Operating hours/Load operation” |
The device provides two different operating hour counters.
|
Operating hours (T_tot) |
This counter keeps running as long as the device is supplied with voltage. |
|
Load operation (T_load) |
This counter is a load counter that starts running from a configurable power threshold (in W). The default setting for the power threshold is 100 W. The value can be configured via the Modbus communication interface. |
Related topics