Inserting Neutral Busbars
The placement of a neutral busbar on a mounting rail requires at least two support brackets which have a neutral busbar placement point. The support brackets mounted on the mounting rail hold the neutral busbar in place (as shown in the following example).
A neutral busbar is placed on the support brackets via the ACCESSORIES > INSERT > Neutral busbar accessory mode.
Once you have placed two ore more support brackets on the mounting rail, selected at least two support brackets and activated the Neutral busbar accessory mode, the insertion points for the neutral busbar are displayed. To place the neutral busbar, select the busbar in the Insertion Center and then click on any insertion point.
Place terminal blocks on neutral busbars / articles between support brackets
You can place terminal blocks on neutral busbars and articles on the mounting rail between support brackets as follows:
| To place... | Do the following... |
|---|---|
| Terminal blocks on a neutral busbar |
Example
|
| Articles on the mounting rail between support brackets | Select the mounting rail and insert the article from the INSERTION CENTER in the usual way.
Example
|

Example