Integration into EU law through the TSI LOC&PAS Fire protection requirements for railway vehicles are defined in an EU specification. Typically, it is referred to as TSI LOC&PAS. Clause 4.2.10.2 of the annex describes the measures to prevent fire. For material requirements, please refer to TSI LOC&PAS Annex J-1, clause 58. In it, EN 45545-2 is referenced as the normative document. Therefore, the binding regulation within the EU is that Part 2 of EN 45545 (EN 45545-2 Railway applications – Fire protection on railway vehicles – Part 2: Requirements for fire behavior of materials and components) is to be applied. Standard EN 45545 consists of seven parts. The fire protection technology requirements are discussed in Part 2, or EN 45545-2. This means that conformity with these requirements is certified in accordance with EN 45545-2. Commission Regulation Commission Regulation (EU) No 1302/2014 of November 18, 2014 concerning a technical specification for interoperability relating to the subsystem “rolling stock – locomotives and passenger rolling stock” of the rail system within the European Union. 4.2.10.2. Measures to prevent fire 4.2.10.2.1. Material requirements (1) The selection of materials and components shall take into account their fire behavior properties, such as flammability, smoke opacity and toxicity. (2) Materials used to construct the rolling stock unit shall comply with the requirements of the specification referenced in Annex J-1, index 58 for the “Operation Category” as defined below: • “Operation Category 2” for Category A passenger rolling stock (including passenger locomotives) • “Operation Category 3” for Category B passenger rolling stock (including passenger locomotives) • “Operation Category 2” for freight locomotives, and self-propelling units designed to carry other payload (mail, freight, etc.) • “Operation Category 1” for OTMs, with requirements limited to areas which are accessible to staff when the unit is in transport running configuration (see Section 2.3 of this TSI) (3) In order to ensure constant product characteristics and manufacturing process, it is required that: • The certificate to prove compliance of a material with the standard, which shall be issued immediately after testing of this material, shall be reviewed every five years • In case there is no change in the product characteristics and manufacturing process, and no change in the requirements (TSI), it is not required to perform new testing of this material. In this case, the certificate needs only to be updated regarding its date of issue J.1 Standards or normative documents TSI Normative document Number Characteristics to be evaluated Section Document no. Mandatory points 58 Measures to prevent fire – material requirements 4.2.10.2.1 EN 45545-2:2013 Relevant section (1) Excerpt from Commission Regulation (EU) No. 1302/2014 of November 18, 2014 (Source: eur-lex.europa.eu) Phoenix Contact 7