News Overview

Surge protection selection made easy

29.05.2017

Configurator: surge protection for MCR technology  

Just two clicks to the right surge protection

The new configurator for surge protection for MCR technology now guides you to a suitable product for your application, with just two clicks.

The configurator came about as part of the new TERMITRAB product range, which has over 100 product versions. Depending on your requirements and application, you can find the right product with TERMITRAB complete. The selection guide provides a quick introduction to the twelve most popular interfaces in MCR technology. Select the signal to be protected with the first click. The second click specifies the desired type. As a result, even at this early stage, you now are shown a recommendation which corresponds to the requirements selected beforehand. Should further restrictions be necessary, such as the correct connection technology, the choice on offer is reduced depending on the selection made. If your interface is not represented in the selection, you can find a suitable surge protective device via the detailed search. Here, you can select your installation, product, and application properties and also find surge protection for your application. In addition to the narrow TERMITRAB complete surge protective devices, the detailed search also includes the intelligent PLUGTRAB PT-IQ protective devices. Furthermore, you will also find the right surge protection for measuring heads in the detailed search.


PHOENIX CONTACT (Pty) Ltd.

36 Lyn Road
P.O. Box 916
ZA-Ferndale 2160
+27/11/801-8200

This website uses cookies, by continuing to browse, you agree to our cookie policy. Read our privacy policy for more information.

Close