News Overview

Bus couplers with certification in accordance with Profinet Spec. 2.3

27.06.2018

Bus couplers, TPS BK  

AXL F PN BK TPS

In PROFINET applications, the Axioline F bus coupler is the link between the Axioline F system and the higher-level Ethernet system. As Phoenix Contact's first PROFINET bus coupler, the TPS version of the device offers certification in accordance with PROFINET Spec. 2.3.

The bus coupler also features PROFIenergy support. This feature uses cut-off mechanisms to save energy when in an inactive state. The web-based management feature, which can be used for retrieving static information (such as technical data), MAC addresses, and dynamic information (such as IP addresses), has been expanded.

The Axioline F station can be started up independently of the higher-level network via the service interface or an Ethernet port on the bus coupler using the Startup+ software.


PHOENIX CONTACT (Pty) Ltd.

36 Lyn Road
P.O. Box 916
ZA-Ferndale 2160
+27/11/801-8200

This website uses cookies, by continuing to browse, you agree to our cookie policy. Read our privacy policy for more information.

Close