News Overview

Two new SIL-rated relays designed for process safety

04/13/2011

Two new SIL-rated relays designed for process safety

Phoenix Contact has expanded its range of safety process relays.

MIDDLETOWN, Pa. – Phoenix Contact has expanded its range of safety process relays. The PSR-FSP2/2x1 and PSR–FSP/2x1 process safety relays are safe interposing relays specifically designed to operate with fail-safe controls in process applications.

The PSR-FSP/2x1 can be used in applications up to a Safety Integrity Level (SIL) 3, and the PSR-FSP2/2x1 can be used for up to a SIL 2 requirement, according to IEC 61508.

The new additions have two normally open safe outputs. The outputs for the PSR-FSP/2x1 are internally redundant, and the outputs for the PSR-FSP2/2x1 are not. Both have a normally closed status contact that can be wired to a SIL-rated controller to perform an automated “proof test.” This can ensure that the targeted SIL level is maintained.

These process safety relays are compatible with “test pulses” and inrush constraints that occur on safe PLC/DCS outputs. The relays measure just 17.5 mm wide. Pluggable and coded screw or spring-cage terminals simplify the wiring.

About Phoenix Contact

Phoenix Contact is a leading developer of industrial electrical and electronic technology. The company's diverse product range includes components and system solutions for industrial and device connection, automation, electronic interface and surge protection. Phoenix Contact GmbH & Co. KG, Blomberg, Germany, operates 47 international subsidiaries, including Phoenix Contact USA in Middletown, Pa. Phoenix Contact’s formal Integrated Management System is registered to ISO quality, environmental and safety standards (ISO 9001:2008, 14001:2004 and OHSAS 18001:2007).

For more information about Phoenix Contact or its products, visit http://www.phoenixcontact.com/usa_home.htm, or call technical service at 800-322-3225, e-mail info@phoenixcon.com.

 

Click for Hi-Res image

 

###


MEDIA INQUIRIES

Molly McGowan
Public Relations Specialist
(717) 944-1300 ext. 3721
Referrer: https://www.google.com/url?sa=t&rct=j&q=&esrc=s&source=web&cd=2&cad=rja&uact=8&ved=2ahUKEwi44ZW4-ZbfAhWDro8KHRP1BckQFjABegQIAhAB&url=https%3A%2F%2Fwww.phoenixcontact.com%2Fonline%2Fportal%2Fus%3F1dmy%26urile%3Dwcm%3Apath%3A%2Fusen%2Fweb%2Fcorporate%2FPress%2Fpress_information%2Fedc81bb8-bce7-4520-87ad-aad8a25ff557&usg=AOvVaw12Q5AHk4VwzIgw7tf_EKyN