News Overview

DIN rail power supplies with real-time monitoring

09/13/2016

New QUINT POWER can be configured specifically to the application

Middletown, Pa. – The newest generation of QUINT POWER power supplies gives control engineers improved configuration and diagnostics to ensure reliable power to the control system. Phoenix Contact has added near-field communications (NFC), real-time monitoring, coordinated surge protection, and a configurable DC output characteristic to the proven QUINT Power line.

With secured NFC, the power supplies can be configured while still in the box. User-definable settings allow monitoring of real-time DC current, power, or voltage using a 4-20 mA analog output. The QUINT power supplies can also be made tamper-proof by locking out the push buttons on the front panel and creating a user-defined password. In addition, operating hours, DC input voltage, overvoltage, and temperature derating can also be monitored with dry contact outputs.


MEDIA INQUIRIES

Molly McGowan
Public Relations Specialist
(717) 944-1300 ext. 3721