News Overview

High-density multi-conductor terminal blocks

08/23/2016

Achieve high wiring density in minimal space

MIDDLETOWN, Pa. – Phoenix Contact introduces PT 2,5/S-QUATTRO terminal blocks.  These four-position terminal blocks occupy the same amount of space as the company’s two-position terminal blocks. This allows for a high wiring density without sacrificing space across the DIN rail.

Up to four 12 AWG conductors can be connected in one feed-through terminal block. The terminal blocks feature Phoenix Contact’s push-in connection technology, for quick, tool-free wiring of the pre-assembled conductors. Ground terminals are also available in the same shape.


MEDIA INQUIRIES

Molly McGowan
Public Relations Specialist
(717) 944-1300 ext. 3721