News Overview

HEAVYCON connector enclosures receive UL 508A certification

06/12/2017

Heavy-duty enclosures for pluggable connector system are certified for interconnection of industrial control panels

Middletown, Pa. – Phoenix Contact’s connector enclosure series HEAVYCON now meets the UL 508A standard for use in industrial control equipment. This certification is important for industrial control cabinet builders in North America who produce UL-certified electrical enclosures. Industrial enclosures that comply with UL 508A standards must use components that have been evaluated and listed by UL as compliant industrial enclosures. These components must have been evaluated by UL and found compliant to attain a Listing for a completed (finished) industrial control panel to comply with the UL 508A Standard.

Additionally, the HEAVYCON connector enclosures are certified for UL Type 4, 4X, and 12 protection categories for panel feed-through connectivity in electrical enclosures. This level of certification ensures that cabinet builders can maintain the original environmental protection rating of the enclosure even after the cut-out is made.  


MEDIA INQUIRIES

Molly McGowan
Public Relations Specialist
(717) 944-1300 ext. 3721