News Overview

CES Multigates handle up to 37 cables

01/11/2016

New Cable Entry System product offers another panel feed-through solution

Middletown, Pa. – Phoenix Contact continues the expansion of its Cable Entry System (CES) product line with the addition of the CES Multigates. These space-saving, metal-reinforced cable entry plates have double-membrane sealing, which ensures a high degree of protection (IP66/67).

The CES Multigates can handle up to 37 cables with an outside dimension of 5 mm up to 60 mm. The CES Multigates offer a low-cost panel feed-through solution, especially where a panel-mounted connector is not preferred.


MEDIA INQUIRIES

Molly McGowan
Public Relations Specialist
(717) 944-1300 ext. 3721