News Overview

Power distribution boxes

05/03/2016

M12 distribution boxes eliminate voltage drop in the field

Middletown, Pa. – Phoenix Contact introduces M12 power distribution boxes designed for field-based power supply voltages of 24 V. These distribution boxes, in combination with standard M12 power cables of 4x10 AWG conductors, can eliminate voltage drop that occurs across long cable runs.

The distributor has four T-coded M12 receptacles with a current load of up to 10 A per channel. Each of the eight channels is equipped with a plug-in fuse. Devices are connected directly via T-coded M12 power cables. Power to the distributor box is supplied via a HEAVYCON Compact plug- connector.


MEDIA INQUIRIES

Molly McGowan
Public Relations Specialist
(717) 944-1300 ext. 3721