News Overview

Designline industrial PCs now available with larger screens and more powerful processor

09/25/2014

Phoenix Contact expands family of IP65 panel PCs with multitouch capability

MIDDLETOWN, Pa. – Phoenix Contact’s Designline industrial PCs are now available with an Intel Core i7 processor in the newly released 18.5- and 21.5-inch screen sizes, as well as the original 15-inch version.  These models are IP65 rated and have a fanless design, making it possible to mount directly on the factory floor.

Because it is safe to use directly on the factory floor, it eliminates the need for additional control cabinet and housing costs. The VESA-mounting hardware mounts securely on the machine. This can improve ergonomics for the operator. For example, the device can be installed at eye level on the front of the machine, and used as a hardware platform for a manufacturing execution system.


MEDIA INQUIRIES

Molly McGowan
Public Relations Specialist
(717) 944-1300 ext. 3721