News Overview

Safe data transmission in the field

03/24/2015

Variant 14 data connectors suitable for harsh environments

MIDDLETOWN, Pa. – The new push-pull Advance data connectors from Phoenix Contact bring future-proof, high-speed cabling directly to the field. The push-pull connection technology complies with ODVA’s Variant 14.

Designed for data rates of up to 10 Gbps, the connectors have IP65/67 protection against dirt, dust, and humidity. With their 360-degree shielding, they are also immune to electromagnetic interference.


MEDIA INQUIRIES

Molly McGowan
Public Relations Specialist
(717) 944-1300 ext. 3721

More Information