News Overview

Software PLC converts industrial PC into a control system

06/20/2012

Software PLC

Using the new software PLC from Phoenix Contact, an industrial PC can handle any control task in real time via Profinet, Interbus or Modbus TCP. Combining PC Worx RT Basic with Phoenix Contact’s Valueline industrial PC equipped with Intel® Core™ 2 Duo processor, the user can configure a high-performance control system with processing times of 0.7 µs for 1K-bit instructions.

In this configuration, one core is dedicated to real-time control tasks programmed using the PC Worx automation software in all five IEC languages.  The remaining core runs existing programs written in a high-level language or other software and hardware running under Windows. Therefore, programming, visualization, communications and control can be combined in just one device. This can reduce wiring costs, control cabinet sizes and the installation footprint in the plant or system.

About Phoenix Contact
Phoenix Contact develops and manufactures industrial electrical and electronic technology products that power, protect, connect and automate systems and equipment for a wide range of industries.  Phoenix Contact GmbH & Co. KG, Blomberg, Germany, operates 47 international subsidiaries, including Phoenix Contact USA in Middletown, Pa.

For more information about Phoenix Contact, visit http://www.phoenixcontact.com, or call technical service at 800-322-3225, e-mail info@phoenixcon.com.


MEDIA INQUIRIES

Molly McGowan
Public Relations Specialist
(717) 944-1300 ext. 3721