News Overview

Energy-efficient industrial PCs

08/06/2015

New features include gull-wing door for easier maintenance and 10-point capacitive multi-touch screen

MIDDLETOWN, Pa. – The new Valueline 2 (VL2) industrial PCs from Phoenix Contact have increased performance power and higher energy efficiency, compared with the legacy Valueline IPCs. The VL2’s design improves usability, incorporates fourth-generation Core-I CPU chipsets, and has an interactive user interface.

The VL2 has a unique gull-wing access door, which reduces maintenance time and also provides easy access to the PCI/PCI-e card. The IPCs have DisplayPort++ for high-resolution images and streaming over a single connector. The 10-point capacitive multi-touch screen allows a more interactive user interface.


MEDIA INQUIRIES

Molly McGowan
Public Relations Specialist
(717) 944-1300 ext. 3721