News Overview

Reduce electrical costs, downtime with electronic measuring instruments

04/16/2013

Electronic energy monitoring  

Phoenix Contact’s new EMpro measuring devices

Reduce electrical costs, downtime with electronic measuring instruments

MIDDLETOWN, Pa. – Phoenix Contact’s new EMpro measuring devices detect, monitor and analyze electrical characteristics, such as voltage, current, power, consumption, harmonics and network asymmetries, of machines and systems.

This data can help engineers make informed decisions about the energy consumption and energy quality of their system. This can lower electrical costs, minimize downtime and reduce harmonic disturbances that can harm sensitive equipment.

EMpro devices work as stand-alone units or can be integrated into an energy management system with plug-in expansion modules. This allows information from EMpro devices to be passed to a control center where the information can be visualized and evaluated. Network communication interfaces include Ethernet, RS-485 and PROFIBUS DP.

In addition, EMpro devices can also be accessed locally, right on the device, thanks to the push-button configuration navigation menu on the front of each device. They also allow on-site setup and configuration, which means system measurement parameters can be set up and changed on the fly. Additionally, information can be collected locally as part of routine maintenance checks.

Two front-panel mount EMpro versions are available: EEM-MA600 and EEM-MA400. Two separate devices are available for DIN rails, EEM-MA250 and EEM-MA200. Each device provides a unique set of features, making it easy for the user to select the EMpro module that meets the needs of the individual task.

 

About Phoenix Contact
Phoenix Contact develops and manufactures industrial electrical and electronic technology products that power, protect, connect and automate systems and equipment for a wide range of industries. Phoenix Contact GmbH & Co. KG, Blomberg, Germany, operates 50 international subsidiaries, including Phoenix Contact USA in Middletown, Pa.

For more information about Phoenix Contact or its products, visit http://www.phoenixcontact.com, or call technical service at 800-322-3225, e-mail info@phoenixcon.com.

###


MEDIA INQUIRIES

Molly McGowan
Public Relations Specialist
(717) 944-1300 ext. 3721