News Overview

Molded cordsets and extension cables for harsh motion

08/24/2011

High-flex M12 cordsets

Phoenix Contact’s new high-flex M12 cordsets can flex up to 15 million bend-cycles.

MIDDLETOWN, Pa. – Phoenix Contact’s new high-flex M12 cordsets can flex up to 15 million bend-cycles. The sensor/actuator cables (SACs) meet the rigorous demands of robotics, motion and C-track installations, where cables need torosional and bending strength beyond standard PUR cable material.

The flexible cordsets’ gray PUR jacket is welding slag-resistant, so that it can flex, bend and twist during the manufacturing process. It is halogen-, silicone- and cadmium-free, and resistant to acids, alkaline solutions and solvents.

The M12 connectors feature a zinc die-cast coupling nut and are available in 3-, 4- and 5-position. The cordsets provide IP65/68/69K protection.

About Phoenix Contact

Phoenix Contact is a leading developer of industrial electrical and electronic technology. The company's diverse product range includes components and system solutions for industrial and device connection, automation, electronic interface and surge protection. Phoenix Contact GmbH & Co. KG, Blomberg, Germany, operates 47 international subsidiaries, including Phoenix Contact USA in Middletown, Pa.

For more information about Phoenix Contact’s SAC products, visit www.phoenixcontact.com/usa_home, or call technical service at 800-322-3225, e-mail info@phoenixcon.com.

 

Click for Hi-Res image

 

###


MEDIA INQUIRIES

Molly McGowan
Public Relations Specialist
(717) 944-1300 ext. 3721