News Overview

Phoenix Contact’s EMpro listed in Go Solar California! initiative

06/04/2015

Energy meter listed as an Eligible System Performance Meter

MIDDLETOWN, Pa. – Phoenix Contact’s EMpro EEM-MA600 energy meter is now listed as an Eligible System Performance Meter with the joint California Public Utility Commission/California Energy Commission’s Go Solar California!  initiative.  This listing allows the meters to be used in solar performance-based incentive (PBI) programs in California and in similar programs throughout the United States that reference the California standards.

EMpro energy meters play a critical role in collecting energy information from the AC circuits commonly found in and around solar electricity installations.  This includes circuits such as those used on the output of inverter stations, to power loads, and for power transmission and distribution in microgrids.  


MEDIA INQUIRIES

Molly McGowan
Public Relations Specialist
(717) 944-1300 ext. 3721