News Overview

Twin Push-in terminal inserts

07/13/2017

Easier connection for heavy-duty connectors in common transmission lines

Middletown, Pa. – The new Twin-PT contact inserts from Phoenix Contact are the first HEAVYCON inserts available with Push-in termination for two conductors per contact. This enables two conductors to be wired in one contact point easily and without special tools.

With these inserts, the user saves time, installation space, and an additional marshaling level. The heavy-duty contact inserts are compatible with many common transmission lines, so they can be combined with other housings and connection mechanisms.  They are well-suited for not only standard housing types but also for box-mounting bases and EVO double-outlet plug housings.


MEDIA INQUIRIES

Molly McGowan
Public Relations Specialist
(717) 944-1300 ext. 3721