News Overview

Crimping pliers with rotating die

06/27/2018

Crimpfox DUO 10 simplifies wire crimping at any angle

Middletown, Pa. – The new Crimpfox DUO 10 crimping pliers from Phoenix Contact are perfect  when diverse workspaces demand flexibility. The Crimpfox’s unique, rotating die permits frontal or lateral insertion of ferrules.

Engaging the color-contrasted release button enables the user to easily rotate the die to the necessary insertion direction, and the Crimpfox’s locking mechanism keeps the die securely in position. The pliers’ self-adjusting mechanism allows them to not only accommodate single ferrules but also reliably accommodate twin ferrules.


MEDIA INQUIRIES

Molly McGowan
Public Relations Specialist
(717) 944-1300 ext. 3721