News Overview

UL approval for M12 power

07.05.2015

M12 power cables  

M12 power cables with UL and CSA approvals

The assembled M12 power cables for S & T codings obtained UL 2237 and CSA C22.2 No. 182.3 approval in April 2015.

The S-coding is specified as 600 V/12 A and the T-coding as 63 V/12 A. Therefore, these may now also be used in the US market. 


PHOENIX CONTACT
SEA Pte. Ltd.

105 Eunos Avenue 3
#04-00
Singapore 409836
+65 6435 9800