Machine builders beware: surge protection is mandatory for machines in parts of the USA. Ensure that your machinery is ready for the new NFPA 79 (2018).
Machine builders and systems manufacturers who export their products to or market their products within North America are subject to the laws and regulations applicable there. One of the most important technical standards apart from the NEC is the 2018 revision of the NFPA 79 standard.
Learn here about which mandatory NFPA 79 requirements are applicable for the use of surge protective devices (SPDs).
The American grid types, voltages, and their frequencies are in part significantly different to those known in Europe, and for historical reasons. Industrial machines are mainly operated on the "3-phase star" and "delta" grid types. There are, however, other grid types: the most common are listed in the following.
Split-phase
This grid type is largely unknown in Europe today. It is created via a secondary-side center tap connection in a single-phase transformer. The center tap connection is grounded, such that the voltage between it and one phase is exactly half of the voltage between the phases. The voltage used is 120 / 240 V.
This grid type is used in almost all households and small office buildings in North America. Small and low-power devices such as computers, televisions and lighting are connected to the 120 V circuit. Devices with higher power requirements, such as air conditioning systems, are connected to the 240 V circuit.
3-phase star
This grid type is very similar to the TM system used in Europe. The live phase conductors are fed from a transformer with star topology, and have a phase shift of 120° each. The neutral point is grounded. Depending on requirements, the neutral conductor may or may not be connected. The voltages used are 277 / 480 V in the USA and Mexico, and 347 / 600 V in Canada.
This grid type is mainly used in industrial applications.
Corner-grounded / ungrounded delta
This grid type is unknown in distribution grids in Europe. The feeding transformer has a delta topology on the secondary side, the phase shift between phases is 120° each. A neutral conductor is not present due to the circuity. The voltages used are 480 V in the USA and Mexico, and 600 V in Canada. Depending on the grounding system, there are two different versions:
Ungrounded delta: The transformer is not grounded on the secondary side. This system behaves similarly to the IT system used in Europe.
Corner-grounded delta: One phase conductor is grounded directly.
This grid type is often used where high powers are required, for example for large motors.
High-leg delta
This grid type is not used in Europe. This grid type is a delta and split phase hybrid. The delta system has a phase to phase voltage of 240 V. In addition, one of the three legs also has a grounded center tap connection. As a result, there are three voltages:
Phase A – N = Phase C – N = 120 V
Phase B – N = 120 V * √3 = 208 V
Between all phases = 240 V
This grid type is used in large office buildings and small industrial buildings. As in the split-phase system, low-power devices (computers, toasters, etc.) are connected to the 120 V circuit, and higher-powered devices (air conditioning systems, etc.) are connected to the 240 V circuit. The 208 V circuit is normally used for lighting.
SPDs are categorized into various types. The types provide information on where in an installation an SPD may be installed. This categorization does not provide information on the performance of the devices or their areas of application in a lightning protection concept. This is not mentioned at all in the listed directives or standards.
Classification | Description |
---|---|
Type 1 SPDs | Type 1 SPDs may be installed downstream of a transformer and upstream of the main fuse or the main disconnector of the installation. |
Type 2 SPDs |
Type 2 SPDs must be installed downstream of the main fuse or main disconnector of the installation. |
Type 3 SPDs |
Type 3 SPDs must have a clearance (= cable length) of at least 10 m to the upstream overcurrent protection or disconnector. |
Products of the VAL-US range are available for the various grid types and voltages. They satisfy the requirements of NFPA 79 because on the one hand, they have a "UL-listed" approval, and on the other hand they can be used universally, thanks to their short-circuit current rating (SCCR) of 200 kA (in accordance with UL 1449 ed. 4).
Surge protection devices that have Type-1 listed approval in accordance with UL 1449 do not need overcurrent protection (1). However, the NEC prescribes that the conductors are to be protected against overcurrent. It can therefore be necessary to equip the conductors to the SPD with overcurrent protection devices (OCPD) (2).
According to NFPA 79, the OCPD is not to be rated or defined by the manufacturer of the installed device, rather by the system planner – in this case by the machine builder. This also applies to SPDs. The procedure for designing the OCPD for surge protective devices is the same as for all other devices. However, since an SPD has no load current, the information specified by the SPD manufacturer can be used for the connecting cable. This information includes both maximum and minimum cross sections, as well as the permitted cable material. Based on this information, the surge protective device can then be designed as usual with the aid of the respective NEC tables.
"$pageName" on