UPDATE magazine

UPDATE is the Phoenix Contact customer magazine and is published as a printed version four times per year. Reports, articles, and interviews provide the customer with an insight into the activities and mindset of Phoenix Contact. Solution-oriented user stories aim to provide an insight into the company from the point of view of the customer and their particular issue.

The magazine must be created using InDesign templates. These are available to download. The templates have been created exclusively for the UPDATE magazine and may only be used for this. The name UPDATE may not be changed.

Freely available Google fonts are necessary for creating the magazine.
Links for downloading the fonts are listed below.

Lutz Odewald is your direct contact for any questions regarding the UPDATE magazine: lodewald@phoenixcontact.com

Downloads

Description Language Updated
UPDATE_en_v02.zip [ZIP, 14.04 MB] English 23.03.2020
Examples.zip [ZIP, 21.69 MB] English 23.03.2020

PHOENIX CONTACT
GmbH & Co. KG

Flachsmarktstraße 8
32825 Blomberg, Germany
+49 5235 3-00