Back to overview

Content teasers

These teasers contain references to the content of the web page and are usually placed in the right column. The country selector is an exception and is placed directly in the content area.

Contact teasers

General contact teaser

All contact teasers have a gradient in the background.

The illustration on the right shows the general contact teaser with and without an image.

If more than one contact is placed in the contact section in the right column of a web page, they are displayed in one teaser box. The contact information is then divided by a one pixel line.

 

Back to top

Country selector teaser

This teaser is only placed on the Phoenix Contact corporate website. It has a gradient with the outline of a world map in the background.

Country selector teaser
Back to top

Cross link teaser

Cross Link teaser

The cross link teaser has a white background. The individual links are divided by a one pixel line. Up to five links can be placed in one cross link teaser.

Back to top

FAQ teaser

FAQ teaser

The FAQ teaser has white background. A one pixel line divides the questions from the FAQ center link.

Back to top

Shopping cart teaser

Shopping cart teaser

This teaser has a grey background (#f2f4f6). If in addition to items in the shopping cart, there a products in the product comparison or in the part list, they will also be displayed. The sections are then divided by a one pixel line.

 

Back to top

Service teaser

Service teaser

The service teaser box has a white background. Downloads, videos, tutorials or forms can be placed in a service teaser box. The different sections are divided by a one pixel line.

Back to top

PHOENIX CONTACT
GmbH & Co. KG

+49 5235 3-41984

Christine Nolte-Dietrich

Christine Nolte-Dietrich

Coordinator Communication Guidelines

This website uses cookies. Read our privacy policy for more information.

Close