Promotional graphics

Graphics for communicating in the marketing environment

Graphics for Phoenix Contact are designed simply so that they can be easily grasped and understood. If possible, the graphics should function without or with very little text. They are always set on a white background to ensure optimum legibility. In the following, you will find a description on how the individual graphic elements can be used, for example, in topologies, diagrams, and charts. The contents are continually updated and are mandatory.

Representation of PHOENIX CONTACT products

2D illustrations  

Examples of 2D illustrations

All products from Phoenix Contact are implemented as vectored 2D illustrations.

Back to top

Applications

3D application objects  

Application object on the left, application world on the right

Products from other companies, machines, and buildings are used as application objects.

In addition to application objects, there are application worlds (landscapes/industries) that can be used for charts (e.g., with marking line). Even complex illustrative graphics such as cross sections of subsections are rendered in this style.

Back to top

Pictograms

Pictograms  

Examples of pictograms

Technologies, communication standards, measuring units, properties etc. are used as vectored pictograms.

Back to top

Logos

Logos  

Examples of logos in graphics

Software logos, technologies, and networks are used as vectored file in the immediate vicinity of the product or cable.

Back to top

Arrows

Arrows  

Example arrows

Arrows without content are shown in black and with a straight point (arrow 9 in Illustrator).

Arrows with text content are shown in color and as block arrows.

Back to top

Text

Text  

Example of text in graphics

Text must be editable and placed in the immediate vicinity of the product or the line. The “PxC GillAltOneMT” in black is used for this.

Back to top

Areas

Areas  

Colors for background areas

To distinguish zones and/or product groups, areas are placed in the background

  • General: 55/20/20/0 (various shades) 
  • Ex: 100/50/0/0 (40%)
  • Safety: 0/0/90/0 (30%)
Back to top

Colors

Colors  

Phoenix Contact house colors

Only house colors in various graduations are used. The background color is always white

CMYK values:

  • Blue-green: 100/0/40/0
  • May green: 50/0/100/0
  • Gray: 55/20/20/0
  • Black and white
Back to top

Connecting lines/cables

Connecting lines/ cables  

Cable colors

  • Do not allow lines to run over elements
  • use specified line colors and in the case of complex graphics, explain in the key
  • Arrange lines vertically and horizontally only, not diagonally
  • Lines lead to the product independent of connections
  • For graphics with more than one wireless connection, dashed lines can be used in addition to the radio waves to illustrate the connections in a clearer way
  • use dotted lines if a cable is possible but not absolutely necessary
  • Use dotted lines on the edge if a cable does not end within the topology of the area illustrated
  • Make sure that lines to other graphics have the same width. Rule of thumb: design the topology on A4 with a line width of 0.75 pt
  • In the case of a dotted line of 0.75 pt, use a gap of 5 pt between the individual dots

 

Back to top

Marking lines

Marking lines  

Examples of marking lines

In the case of markings or the depiction of a product within a 3D application world or a 3D application object, a neutral black or turquoise-colored line is used with a period at the end. The period can be adjusted in Adobe Illustrator under “Arrow heads”, whereby the scaling is 70%.

Back to top

Radio waves

Radio waves  

Examples of radio waves

Wireless connections are identified by three black arcs.

Tip: the radio waves are stored in the vectorized image in the database under the number a_0059512.

Back to top

Effects

All graphics (diagrams and topologies) except application objects and worlds are two-dimensional and used without effects such as shadowing or gloss.

 

Back to top

Photos

Photos are not used in graphics.

Back to top

PHOENIX CONTACT
GmbH & Co. KG

Flachsmarktstraße 8
32825 Blomberg, Germany
+49 5235 3-00