Lightboxes

To allow the Phoenix Contact booth to be identified from a distance, we use lightboxes (height 1.20 m/47.2 inches) with the Phoenix Contact logo and the signal chain on the surrounding supports as a standard element. Unless it is necessary to maintain a distance of 1.00 m (39.4 inches), the lightboxes allow for an overhead structure extending up to the edges of the booth.

PHOENIX CONTACT
GmbH & Co. KG

+49 5235 3-41984

Christine Nolte-Dietrich

Christine Nolte-Dietrich

Coordinator Communication Guidelines

This website uses cookies. Read our privacy policy for more information.

Close