Back to overview

App icon

Every app requires an individual application icon that represents the app on the home screen of the end device and in the respective app store. Example application icons have been developed based on the currently applicable requirements of the three operating systems; they define the basic layout of an icon motif and include recognizable branding. A separate app icon will be designed for every new app, which can be clearly associated with the Phoenix Contact brand.

To ensure clear recognition, the Phoenix Contact logo must be placed on a light gray gradient in the top part of the image. The customizable area below contains an app-specific name in white text centered on the “Signal chain, left color”. 

Description Updated
App icon template master 1024 x 1024 [PSD, 0.67 MB] 22.08.2017

App icon dimensioning

App icon dimensioning  

App icon dimensioning

The layout of the app icon is identical for all operating systems. The following percentage dimensioning and spacing applies.

The output of the final image file for the app stores should appear as follows.

  • Color mode: RGB
  • Size: 1024 x 1024 pixels
  • Resolution: 72 dpi
  • File format: JPG, PNG

Transfer to operating systems

The final implementation of an app icon for the various app stores is in line with the specific requirements of the individual operating systems. For the required dimensions or image formats, refer to the currently applicable guidelines for iOS, Android, and Windows. A prototype app icon has been implemented for all three operating systems in accordance with the current guidelines (as of 06/2017); each of these icons has a distinctive border. 

Transfer to operating systems  

Transfer to operating systems

App icon in communication

App icon in communication  

App icon in communication

To promote the Phoenix Contact apps on various media platforms, the application icons must be presented uniformly. To do this, mask the created graphic with the vector form (rounded corners) “App_Icon_Communication”.


Back to overview
Further information

PHOENIX CONTACT
GmbH & Co. KG

Flachsmarktstraße 8
32825 Blomberg, Germany
+49 5235 3-00