Architecture

Phoenix Contact's architecture is based on the Bauhaus style and uses steel, glass and concrete materials. Facades are designed correspondingly in discreet gray and white tones. Our architecture conveys a technical feel, consistent with Phoenix Contact's products and production facilities. Stylistic elements are cubistic layouts, walls and windows are at right angles, roof surfaces are horizontal.

In general, the following architectural characteristics apply:

  • solid construction
  • geometric clarity
  • durable materials
  • technical surfaces
  • color-free optics

This uniform technical scheme, combined with carefully tended green areas, documents our distinct style, and shows the same precision and quality standards as do our products and production facilities.

Implementation must be country-sensitive. Country specific conditions and cultural influences must be taken into consideration, while conforming to the specified style.

The Phoenix Contact style is more pronounced in buildings owned, rather than rented, by the company. It is nevertheless possible even in the case of rented buildings to influence design towards functionalism and compliance with the corporate identity.

PHOENIX CONTACT
GmbH & Co. KG

+49 5235 3-41984

Christine Nolte-Dietrich

Christine Nolte-Dietrich

Coordinator Communication Guidelines