News Overview

Compact Bluetooth wireless module for wireless signal transmission

28.03.2017

Wireless-MUX – the wireless signal cable

[4938] The Wireless-MUX Bluetooth wireless module from Phoenix Contact transmits 16 digital and two analog signals bidirectionally, which means that it can replace a 40-wire signal cable.

The new products feature a state-of-the-art hardware platform, based on the latest Bluetooth standard 4.0, and offer analog channels with a higher level of accuracy.

As part of the harmonization of Phoenix Contact's wireless modules, the antenna connection has been changed from MCX to RSMA and moved to the top in order to optimize the space used in the control cabinet.

The Wireless-MUX system does not require additional configuration or settings, it can simply be started up. It features fast connection establishment and a low delay time. The wireless system is robust and reliable and supports interference-free operation alongside WLAN. The link quality indicator provides the user with constant information regarding the connection quality.