News Overview

App supports 4G devices

17.07.2019

TC MOBILE I/O X200-4G signaling module with updated app

[5143] The TC MOBILE I/O app supports the use of the TC MOBILE I/O X200 alarm and remote control module by enabling SMS commands to be triggered with just a click and displaying the current device status clearly to the user.

With the update, the app also supports the new module versions recently launched on the market, which offer the latest 4G mobile technology (LTE CAT1) and 2G fallback (GSM/GPRS/EDGE).

The TC MOBILE signaling system is ideal for sending simple SMS and e-mail alerts containing digital and analog values as well as for switching relay outputs. The module is controlled via SMS commands that can be sent either by the technician out in the field via mobile phone or via a mobile router in the control room. The app saves you having to manually type out an SMS text, provides additional information such as the device documentation, and clearly displays the device status.


PHOENIX CONTACT
GmbH & Co. KG

Corporate Communications
Flachsmarktstr. 8
D-32825 Blomberg
+49 5235 3-41240