News Overview

Surge protection selection made easy

29.05.2017

Configurator: surge protection for MCR technology

[4957] The new “Surge protection for MCR technology” configurator from Phoenix Contact now guides you to a suitable product for the application at hand, with just two clicks.

The configurator came about as part of the new Termitrab complete product range, which has over 100 product versions. Depending on customer requirements and the application, this configurator enables you to find suitable products from the product range.

The selection guide provides a quick introduction to the most popular interfaces in MCR technology. The first click selects the signal to be protected, the second click specifies the desired type. The hitlist includes a product recommendation that corresponds to the requirements previously selected. If the interface that was searched for is not included in the initial selection, there is a further detailed search. Selecting the corresponding installation, product, and application properties once again leads to a corresponding solution here.

In addition to the narrow Termitrab complete surge protective devices, the detailed search also includes the intelligent Plugtrab PT-IQ protective devices, as well as surge protection for Surgetrab measuring heads. The new configurator can be accessed by entering web code #1389 into the Phoenix Contact website search field.