News Overview

Current indicator lever-type disconnect terminal block with Push-in connection

27.06.2018

Clearly identify malfunctions and line breaks in the operating state.

[5049] Phoenix Contact now offers the new PT 4-HE-ILA 100 current indicator terminal with Push-in connection technology to help clearly identify malfunctions and line breaks in the operating state.

The voltage drop is evaluated at a Zener diode in reverse direction and is indicated by an LED. The circuit can be safely disconnected using the disconnect lever. The compact design of the terminal block saves space in the control cabinet. It is identical in shape and bridgeable to standard terminal blocks. Testing can be done conveniently using a test point accessible from both sides. The marking options for all of the terminal points and the disconnect lever ensure a clear view of the arrangement.