News Overview

Expansion modules for PLCnext Control controllers

01.04.2019

Left-alignable Ethernet interface

[5117] From now on, users can operate even more individual requirements with the PLCnext Control controllers from the Axiocontrol series from Phoenix Contact: The interfaces of the PLCnext Control can be adjusted using expansion modules.

These expansion modules are then connected to the left side of the controller and operated. The first module provides an extra Ethernet interface with an additional MAC address. Configuration is performed via the PLCnext Engineer software.

In the future, additional bus-specific modules for INTERBUS and PROFIBUS will be added to this Ethernet expansion module. Both variants will include a master function to connect existing INTERBUS and PROFIBUS participants.