News Overview

Panel PCs in new format

18.09.2014

Panel PC

[4657] Phoenix Contact is extending its range of Embeddedline panel PCs with 4:3 format displays.

Previously, the Embeddedline series from Phoenix Contact was only provided with 16:9 displays. These devices are now also available in 4:3 format. As such, existing visualizations can also be implemented in future using this range. The devices with 4:3 format are available in 10", 12", and 15". The new panel PCs can be configured in a similar way to the Embeddedline PCs in widescreen format, so that they can be individually assembled in terms of the processor, mass storage, and operating system.